×

You're close to some great linear motion content!

First Name
Last Name
Company Name
!
Thank you!
Error - something went wrong!
   

The ACME Lead Screw System

September 14, 2017

One of the most common lead screw geometries in North American manufacturing is the ACME lead screw system. Designed with a trapezoidal shape, a flank angle of 29 degrees and a higher pitch than fastening screws, ACME lead screws were made for applications requiring frequent positioning, including power transmission applications moving high axial loads. High-performance plastic ACME nuts are also ideal to use in an ACME system. 

Learn about speeds and loads, lead screw geometry, nut materials, benefits of an ACME system, relevant industries and more. 

Previous Flipbook
Cell-stacking technology could change the future of organ transplant waiting lists
Cell-stacking technology could change the future of organ transplant waiting lists

Next Video
Heavy Duty Stainless Steel Linear Guide | drylin® HTS
Heavy Duty Stainless Steel Linear Guide | drylin® HTS

See how drylin HTS stands up against fire and being run over by a truck!

Want to see if igus lead screws will work for you?

See tech specs