×

You're close to some great linear motion content!

First Name
Last Name
Company Name
!
Thank you!
Error - something went wrong!
   

The ACME Lead Screw System

September 14, 2017

One of the most common lead screw geometries in North American manufacturing is the ACME lead screw system. Designed with a trapezoidal shape, a flank angle of 29 degrees and a higher pitch than fastening screws, ACME lead screws were made for applications requiring frequent positioning, including power transmission applications moving high axial loads. High-performance plastic ACME nuts are also ideal to use in an ACME system. 

Learn about speeds and loads, lead screw geometry, nut materials, benefits of an ACME system, relevant industries and more. 

Previous Flipbook
The levitating effect: New exoskeleton is transforming production
The levitating effect: New exoskeleton is transforming production

Next Video
Cablenews – straight from the igus® laboratory – SPS2016
Cablenews – straight from the igus® laboratory – SPS2016

Directly from the test lab to the exhibition at SPS2016 Rainer Rossel, Head of the igus® chainflex® divisio...