Chain breakage is easily detected and solved using smart energy chains

December 21, 2018

The EC.B break detection sensor from igus® smart plastics division reduces the amount of work of maintenance technicians tasked with looking after crane installations and gantries. This applies from classical smaller indoor cranes in production facilities right up to the huge cranes used in ship-building. The EC.B sensor can detect breakage of a chain link caused by parts falling into the system or similar. In the past, this problem was often a critical factor in the failure of a crane as breakage of a chain link automatically leads to overloading and failure of the opposite side.

Previous Video
Installation of an igus® guidefast control system on a crane girder
Installation of an igus® guidefast control system on a crane girder

This video walks through the installation of an igus® guidefast® trough on a crane girder.

Next Video
Port of Virginia Crane Technology [Preview]
Port of Virginia Crane Technology [Preview]