Other content in this Stream
Linear bearing systems create sliding technology for maximum design potential. The tribologically-optimized plastic liners, self-lubricating bearings customizable rails allow engineers the abi
Over the past 3 decades, there has been a revolution in the advancement and use of highly engineered plastics in bearing applications. In this tech talk, uncover the top 5 reasons to replace PTFE-line
Choose the right shaft for your bearing is equally important as the bearings material when it comes to the lifespan of your bearings.
We compared true maintenance-free designs with alternative designs. Discover what goes into creating a truly maintenance-free pivot.
We break down the components of a modern ball bearing, and explain what type of bearing materials are best for certain environments.
Bearing lubrication can transfer bacteria and other contaminants between food. See what bearings you can use that are compliant
A rapidly growing number of industries have replaced traditional metal bearings with advanced plastic materials. However, some engineers without experience with these plastic materials may be reluctan
Learn how making the switch from metal to composite plastic bearings can eliminate bearing maintenance, increase service life, reduce corrosion and wear, and more.
In this white paper, uncover common misconceptions and learn the true reliability of tribologically-optimized plastic bearings.

In this webinar, you'll discover the reliability of plastic bearings, learn about the course of real-life testing they endure to prove their strength, find out about the range of specialized materials

igus iglide® plastic bushings can be found in wide range of applications across many industries including food processing, medical, marine, textile, agriculture, automotive, filling machines, drive te

An in-depth look at iglide® plastic bearing materials from igus®.
This white paper explains how much it actually costs to lubricate a ball bearing and the cost saving benefits of switching to a self-lubricating plastic bearing.

Try it out for yourself! www.igus.com

Take a look inside the igus® self-lubricating bearings lab. Over 15,000 tribology tests are run each year in our massive 29,600 square foot lab. Learn more at www.igus.com/testlab.
Learn how hybrid linear bearings can reduce bearing friction, reduce required drive force, and allow system functionality without conforming to the 2:1 rule.

A showcase of special applications in which igus® iglide® bearings improve upon standard metal bearings. iglide® is a low cost, self-lubricated, dirt resistant, UV resistant, and light weight solution
It’s easy to use the same steel or bronze bearings on your machine, but could they be costing you more in the long run?

This video introduces the igus dry-tech bearings box at MD&M West. This box helps engineers choose the right bearing for almost any application. This includes dirty environments, low coefficient of fr