Sliding vs Rolling: Benefits of Plastic Linear Bearings

Prefer to watch the webinar? Here you go: https://www.youtube.com/watch?v=SLXX4kHNp5s The topic of today's webinar is sliding versus rolling: the benefits of plastic linear bearings. We are going to discuss how to correctly implement plastic linear plain bearings into applications where you are likely more familiar with designing in recirculating ball bearings. Implementing plastic linear bearings is a way to help you improve the lifetime of your equipment, reduce costs and eliminate the need for grease from your applications. This presentation is technical in nature and there are a number of key takeaways:
  1. How composite plastic bearings are made
  2. How what we call motion plastics or engineered plastics differs from simpler commercial plastics available on the market
  3. How they work
  4. How they differ from recirculating ball bearings
  5. How they can help reduce the maintenance and downtime associated with lubrication or lubrication-related failures in the field
  6. How they are able to offer cost reductions through self-lubrication
  7. How to properly implement plastic linear bearings into your designs
  8. Different application examples (so you can better understand when and where to use plastic bearings)
At igus, we aren't necessarily inventing new plastics, but we are developing new tribologically optimized, composite plastic compounds that are specially formulated for bearing applications.

A Note on Tribology

Tribology is a core competency that igus focuses on when creating motion plastics. We study mating surfaces, including the wear and the frictional characteristics of these systems. Basically, we try to develop materials that enhance plastics for bearings. A lot of you are used to using parts that require oil and maintenance. If we can reduce oil costs and wear, we might be able to reduce the overall cost of your systems and applications.

Design of Composite Plastic Bearings

We start with base polymers. These polymers could be a POM or PA base. These polymers are responsible for the main mechanical properties of the bearing. It gives the core strength, carrying capability and the core temperature limits of the product. To that, we add a matrix of solid lubrication. Sometimes that takes the form of PTFE fillers. There are other types of solid lubricants, sometimes silicone, that we add to the bearing materials. These lubricants are responsible for reducing friction in the application. We also add strengthening fibers and reinforcement compounds into the base material, which not only help the load carrying capability, but they also help the wear resistance of the parts. This bearing itself is only one half of the equation in a bearing system. The other half of the equation is the shaft or the rail that the bearing is riding against.

Counter Phase and Washdowns

The counter phase occurs when transfer of the bearing material goes into the microfinish of the shaft. What’s important to understand is that once the transfer is made, it can't be washed away. This is a core benefit of plastic parts. These parts work well in applications that are submerged or submitted to washdown environments. In a lot of bottling lines, caustic washdowns take place. If you were trying to use bearings that required wet lubrication, as soon as they were sprayed with the washdown, the bearing lubricants would be leached from the system. This leaching means that in order to maintain the whole line, you would need to re-administer lubrication. Plastic bearings don't require this and are well-suited for applications that have chemical washdown or are submerged in water.

Geometry of Plastic Parts

A lot of people are used to seeing plastic bearings in a simple sleeve or flanged form. However, plastic linear bearings can also have features on the outer diameter that can help anti-rotation in applications. These features can keep the parts mechanically fixed in the axial direction. Grooves are an important feature of the inner diameter (ID) of plastic bearings from igus. Grooves serve two purposes. One is that they are dirt channels. If your application is heavily contaminated by dirt, soil or particles, grooves can act as a channel for that media. Even more critically, they're able to reduce the amount of thermal expansion of the ID of the bearing towards the shaft. That means that we can produce parts to a tighter tolerance, with a tighter clearance in the application than you could with a standard sleeve bearing. A standard sleeve bearing, as it swells, would only have one way to go. That's towards the shaft, which could cause bearing failure. Therefore, the grooves on the ID are a critical feature of a plastic thermoplastic bearing.

How igus Plastics Compare to Generic Plastics

Wear rates of iglide plastic linear bearings compared to three other common materials

The above chart is a frictional com parison between generic plastics and of a composite plastic we call iglide J, which happens to be a linear bearing specialist from the igus line of motion plastics. Note how the friction characteristics are different from the simpler plastics on the right such as PEEK or POM. You will see that iglide J has better friction on anodized aluminum and case-hardened steel, which is probably the most common linear bearing shaft material. The advances of tribology shine when compared to simple plastics, not only with friction but also with wear. So, we've now discussed how plastic bearings are made, how the technology works and how they compare to simpler plastics. Now it's very important for us to compare them to the most common linear bearing systems available, which are recirculating ball bearings.

Plastic Linear Bearings vs. Recirculating Ball Bearings

There are frictional differences between plastic sliding bearings and linear recirculating ball bearings. Recirculating ball bearings have a coefficient of friction of 0.01, whereas plastic sliding bearings have a coefficient of friction between 0.16 and 0.25.

Pros and cons list comparing traditional rolling ball bearings to iglide sliding plastic linear bearings

The above slide highlights the main benefits of each part, which are in green and the main problems with each part, in red. Linear recirculating ball bearings always require wet lubricant that might be grease or oil. Plastic bearings don't require that external lubrication, since they are self-lubricating. And since they don't require lubrication like ball bearings, they work really well in dirty or clean environments. They offer cost reductions and they're ideal for lightweight applications as well as short strokes.  Plastic bearings are better suited for positioning and pick and place applications. Recirculating ball bearings are ideal for high precision applications or applications that have high speeds in conjunction with high loads. They also offer advantages in highly cantilevered applications outside of what we call the 2:1 ratio, which we'll discuss later. Ball bearings, because of their low coefficient of friction, enable applications that are hand powered to be moved easier. Ball bearings are also low clearance since they use rolling technology instead of sliding technology. They can be made to smaller tolerances, so that really positions them well in environments like machine tools, machining or moving small parts into very small places. Some of the negatives are that they can be cost prohibitive for a lot of applications, they have problems with vibrations, require constant maintenance and lubrication, and they can be loud. And they must use hardened shafting. Plastic bearings can perform different types of motion profiles, such as linear and rotating. At the same time, they’re low weight and they can also be used on soft shafts, which is very important in a lot of industries that are using stainless. Ball bearings require 440c hardened shafting, which can pit and corrode, whereas plastic parts can use 300 series stainless steel. This range of steel is easier to machine and has much better corrosion resistance. Some of the problems, however, with plastic parts is that they have higher coefficients of friction than ball bearings, as well as higher clearances, due to the fact that they're sliding instead of rolling. Because plastic bearings do not operate on the same point-to-point contact as ball bearings do, they reduce the surface pressure in any given application. That makes them better in high static load environments or applications with shock loads that might cause the balls to embed into the shaft, causing galling – same with vibrations and edge loads. Also, ball bearings are not really well suited for high acceleration applications due to the inertia in the balls. A lot of times, I’ll visit customers and I’ll see shafts with damage at both the beginning and the end of travel. That's mainly due to high accelerations where the motor starts moving but the balls, due to inertia problems, start sliding first and then catch up as it goes along. Same thing happens during the deceleration process or when the motor reverses course. The balls are moving in the opposite direction of the bearing itself, damaging the shaft. Plastic plain bearings don't have that type of problem. There are no real limits to the acceleration profiles for plastic parts. Don't just take igus’ word for it about plastic bearings and how they can save and reduce maintenance costs. We like to talk about that a lot, but basically any study done on bearing systems will tell you that the number one problem with any bearing system is due to lubrication-related failures. That could be from the parts not being maintained correctly, the grease not being administered at the right time or improperly, or there could be an environmental problem where using grease and dirt cause an ingress of contaminants into the ball bearing. Since composite linear plastic bearings don't require these external lubricants, there is not the main problem of lubrication-related failure. They also don't require the ancillary equipment required to keep systems clean. Plastic bearings don't require any special seals or wipers to keep lubrication out and/or dust out of the system. They are self-cleaning. If you look at this application photograph below, you'll see two composite linear bearing rails that are in a cut-off saw for particle board.

Graphic demonstrating self-wiping properties of plastic linear bearings

You can see that the portion where the bearings travel over is clean. That's because the bearings have self-wiping attributes. If you look at the end of the shaft where the bearings don't travel, you'll see that the contamination is stuck to it. So the important thing to take away here is that plastic bearings are self-cleaning. They won't have lubrication-related problems like linear ball bearings can. A sometimes overlooked benefit that plastic bearings offer versus recirculating ball bearings is their weight reduction. This is important for not only industries where you're trying to save weight like in the automotive industry or aircraft interiors, but it's also important in any application where you have a gantry system and one linear bearing axis is moving on another. It’s important to keep the weight down in any machine design that reduces the inertia and the moments in the system. Plastic bearings reduce the stresses on the motors or on the pulleys or on anything else in the application. You can use plastic bearings to help you to lower the weight of your designs as well. As well as weight reduction, plastic bearings also have some unique designs that enable you to lower the overall profile of the linear bearing system in an application. How to Properly Use Plastic Linear Bearings (Design Guide): The 2:1 Rule Now I'd like to get into the proper ways to implement plastic bearings into your applications. There's a couple of key things that have to be observed when working with sliding bearings instead of rolling bearings and we're going to go over those things right now. Perhaps the most critical rule to follow when designing with plastic sliding bearings, or any type of sliding bearings that doesn't use grease or lubricant, is what we call the 2:1 rule (see the video here). The rule states that any acting force on the system, which is usually a drive force or a payload, has to be within a distance of two times the bearing length on the rail that's closest to the drive side on that drive. The rail that’s closest to the drive side is what we call the fixed bearing side. We call the farther side the floating bearing side.

Design Guide: Fixed and Floating Bearings

Square shaped or profile guides are the easiest ones to adjust as floating bearings. We simply either remove the plastic pads from the sides or top, depending on the orientation of the application or we mold the plastic parts narrower. This enables the part to carry a load in the direction of gravity but slide and float towards the other rail. This design not only helps with misalignments but also helps optimize the system under the 2:1 rule. In round shaft or round rail designs, in an adapter form, which would have the same dimensional sizing as a recirculating ball bearing, we actually reduce the outer diameter of the adapter itself and add a little crowned feature. This feature enables a plus or minus half degree of angular misalignment forgiveness. Usually o-rings are provided, which help reduce any noise caused by the metal-on-metal contact of the adapter pivoting inside of the housing. What’s critical about fixed and floating bearings and how they can improve your design is to optimize the 2:1 ratio, which in turn reduces the drive power that the system needs in order to move. This reduction increases the likelihood that you can move your application by hand. You may be able to undersize your motor as well. This minimizes the wear on the bearing and it also increases the maximum permissible velocity of the system. Overall, contrary to what you might think, floating bearings help to maintain a better precision and clearance in a linear system. These bearings also help to compensate for angular misalignment in the rails or shafts.

Explanation of the 2:1 rule for plastic linear bearings

Design Guide: Linear Bearing System Configurator

To help make it easier for engineers to specify plastic bearings and to make sure they're going to work correctly in their application, igus offers an online expert system we call the drylin expert 2.0. You're able to choose the geometry that you'd like to use in your application, then you're able to model it up in our software. After that model, you receive a series of results and get to understand better if the parts will move smoothly again. You can also understand and get an idea of the clearance and wear in the application, as well as get an idea of the drive force. One really critical function of this software is the fact that you're able to move. You're able to tell the system where the center of gravity is for your application and where you intend on driving it in your application. It's going to measure those coordinates from a pre-set zero-point established in the software and after you put in your load acceleration and your expected lifetime travel, you're able to take the next step. This is a real clear way to see it on the modeling software itself. After you input all your data, it's time to check out the results, request part numbers, and download CAD files right off the Internet. This system is very easy to use.

Plastic Plain Bearing Applications

Two core industries for igus motion plastics are definitely lab automation and fluid handling. A lot of different lab machines rely on linear plastic sliding parts. Pipettes is another instance but the fact that there's no lubrication makes them really well-suited for any type of use around scientific chemicals or chemistry. There's no lubrication to leach into the samples. It keeps the immediate lab environment clean. Here's an application on a blood analyzer. On the elevator mechanism, we replaced ball bearings, primarily due to the fact there was no need for oil. Not only did they use plastic bearings, but they also coupled that with aluminum shafting, which is again the best mating surface for plastic sliding parts. The upfront cost savings to the customer was $36K per year compared to the price of bearings. Therefore, not only was there a technical advantage, there was a price advantage as well. Savings like this are part of the igus mission. Aside from linear parts, 3D printers use a lot of plastic bushings for pivoting or rotary applications, as well as plastic lead screws and nuts. Also, one absolutely core industry for igus’ plastic composite bearings is the packaging machinery business. One classic application is the welding jaws on vertical form fill seal machines. These are basically machines that have a hopper above that dispenses chips into a bag. These welding jaws are parts that close usually with heat. These types of applications can be nasty environments, depending on what the end user is packaging. The items to be packed could be harsh substances like onions, chips, mulch or all sorts of different media. Plastic bearings, due to their lack of wet lubricant, thrive in these applications.

The drylin Product Family

Here's an overall comprehensive look at the drylin product family by igus.

the drylin product family, which includes plastic linear bearings, linear rails, and lead screws & nuts

Starting from the top left, you'll notice a series of round parts. These are interchangeable with recirculating ball bearings. We also offer aluminum, steel and stainless shafting, in both inch and metric sizes. Below you'll see drylin T, which is interchangeable with common profile rails that are on the market, but again uses plastic sliding parts instead of ball bearings. In the top center, a product line we've discussed a little bit earlier is our drylin W toolkit, which is a unique and flexible offering by igus as far as different geometries, materials for engineers and setting a new standard for a linear bearing product. Below that you'll see a belt drive with a motor. That's just a reminder that igus can also provide fully actuated solution with either toothed belt gears, lead screw drives or gear racks with stepper motors or DC motors, as well as cables. On the top right is drylin N, which is a series of low cost, low profile linear slides and the bottom right is drylin SD. That's our screw drive technology, which is available in acme, trapezoidal (featuring zero-backlash and anti-backlash functions), as well as dryspin, which is our own proprietary high helix lead screw geometry. Want to discuss your linear bearings application with a product expert? Contact us here, call us at 1-800-521-2747 or visit our linear bearings & slides page today.

Shizu Yamaguchi