Flange Solutions
Most Recent Videos

igus® solutions for public transportation
See how igus® products can help public transportation run smooth and lubrication free! For more information visit: https://www.igus.com/info/industries-public-transport

Simplest motor control system for stepper, DC, and EC/BLDC motors
The igus dryve is easy to connect and utilizes a web-based interface. It is easy to configure, has 32 positions, 5 operating modes, 6 position types, and has a library of online video tutorials.

Chain breakage is easily detected and solved using smart energy chains
The EC.B break detection sensor from igus® smart plastics division reduces the amount of work of maintenance technicians tasked with looking after crane installations and gantries. This applies from c

Hidden cable damage detected by smart plastics sensor at an early stage
The CF.Q sensor from the igus smart plastics division indicates changes in the electrical properties; and allows detection of impending cable failure in advance. The electrician then decides what prio

Smart plastics sensors measure push/pull forces in energy chains
Using the EC.P sensor saves maintenance personnel from having to travel many miles - thanks to real-time status information always being available inside the isense system. The push/pull sensor and de

New igus chainflex cable innovations presented at SPS 2018
Head of igus chainflex cables, Rainer Rössel, explains the new and available lines of chainflex cables. These new cables include robot cables with a torsion angle of ±360 degrees, a new line of heat r

How to install an igus twisterchain on a six-axis robot
Step-by-step walk through of the installation of an igus twisterchain for the 1st axis on a six-axis robot

dryve D3, DC-Motor Control System Assembly
We are excited to share the new DC-Motor Control System designed to be used with or without higher level controls. The following is a step- by- step guide to get your igus actuator moving with the new

How to assemble a zero or anti-backlash nut
In this video igus® drylin® product Specialist, Nick Isabella, demonstrates how to install a zero backlash nut on a lead screw. Zero backlash or anti-backlash assemblies employ two nuts, which are for

Energy chains for stage and theater applications
Watch the full video here: https://www.youtube.com/watch?v=Jt4yEIIaeBw Or visit our website: https://www.igus.com/info/industries-theatre

igus® House of Horrors - powered by the drylin D3
Late at night when all igus employees have gone home, something creepy is going on in the drylin® laboratory. The drylin® dryve D3 DC motor controller, drylin® W slides, and some creative props make a

How to switch to plastic bearings
drylin® T linear guide systems were specially developed for applications in automation and handling systems. The design objective was a rugged linear guide for application in the most diverse - and al

drylin® W toolkit by igus®
The drylin® W toolkit is one of our most popular solutions. See why you should make the switch to self-lubricating linear motion! For more information visit https://www.igus.com

Cable reels replaced with new Energy Chain solution at Kauffman Center for the Performing Arts
The Kauffman Center for the Performing Arts is the leading opera and performing arts venue in Kansas City, MO. Since its opening in 2011, it has hosted over 2.5 million guests. To power the overhead s

igus® smart plastics for Industry 4.0 - e-chain® monitoring systems
Product Manager, Scott Parker, introduces igus® inc Smart Plastic initiatives towards industry 4.0. Including wear, break, push pull force, and conductor care, igus® is moving customers towards predi

New! delta robot from igus® at IMTS 2018
The igus® delta robot provides a thrifty and simple automation solution for pick-and-place tasks. These maintenance-free, lightweight robots start at $6,200 and are available in easy-to-assemble kits

igus® Traveling Trade Show
For more information on the igus® Traveling Trade Show or to book a stop, visit www.igusontour.com

triflex® - RSE linear retraction system
The igus triflex® - RSE linear retraction system is the newest technology available in the marketplace. It will reduce cable lengths and improve productivity. For more information visit: https://www.

IMTS 2018 - Highlights
A quick recap of our biggest show to date - IMTS 2018! Thank you to all who had the chance to stop by. If you have any further questions from the show, do not hesitate to contact us at: https://w

delta robot from igus®