PTFE-free materials: What options does industrial coating offer?

On this page

What substances are contained in the materials you use? What requirements must they meet in a specific application? And which alternatives are available without compromising on wear protection or technical performance?

These questions are becoming increasingly important when selecting industrial coatings. PFAS and PTFE, in particular, are receiving greater attention in connection with potential regulatory restrictions. For companies, this makes it increasingly important to understand the material properties of their coatings and assess suitable alternatives for their applications.

Cover of a white paper about PFAS and some of the legislation and restrictions around its use

PTFE and PFAS: What do they mean for coatings?

PFAS stands for per- and polyfluoroalkyl substances. This group comprises numerous chemical compounds used in a wide range of industrial applications due to their specific properties.

PTFE is a fluoropolymer that belongs to the PFAS group. In coatings, it is used, among other things, for its friction-reducing properties.

Regulatory developments surrounding PFAS are making material selection more complex. However, not all PFAS substances should be assessed in the same way. The relevant requirements depend on the substances involved, the applicable regulations and the specific field of application.

This makes coating materials that combine defined material properties with a targeted selection of ingredients all the more important, helping meet the requirements of individual components and applications.

With iglide® IC-01PF and IC-02PF, igus® offers two new coating powders that are PTFE-free and tested for selected PFAS substances.

For industry, the key question is: How can the required technical properties be achieved when PTFE needs to be avoided in material selection?

igus has been exploring alternatives to PTFE for some time and already offers suitable materials across different product ranges. Industrial polymer coatings are part of this portfolio. With the new coating materials IC-01PF and IC-02PF, two additional options are now available.

Array of powder coating materials from igus

PTFE-free coating: Selecting materials for specific requirements

When selecting a coating, its composition is only one consideration. It must also meet the requirements of the intended application. These may include sliding properties, wear protection and protection of metallic surfaces against corrosion.

The new iglide coating powders IC-01PF and IC-02PF combine these requirements with a PTFE-free material composition. Both variants have been tested for 96 selected PFAS substances.

iglide IC-01PF: This powder is suitable for metallic components whose surfaces need protection against wear and improved sliding properties.

iglide IC-02PF: The black variant offers the same fundamental benefits for surface coating and adds another color option to the portfolio.

What are the key benefits?

  • PTFE-free: For applications where PTFE needs to be avoided.
  • Tested for selected PFAS substances: Tested for 96 selected PFAS substances.
  • Wear protection: For surfaces and components subject to wear.
  • Corrosion protection: Confirmed in a 480-hour salt spray test in accordance with DIN EN ISO 9227.
  • Two new color options: IC-01PF in white and IC-02PF in black, complementing the existing range in gray and blue.

Coating can extend component service life and reduce the need for replacement. It can also eliminate the need for lubrication, prevent material build-up on coated surfaces and support favorable sliding behavior between contacting components.

A spray gun spraying coating powder

More than two new coating materials

iglide IC-01PF and IC-02PF complement a coating portfolio that includes additional materials for different operating conditions:

iglide IC-04 is available in gray and designed for applications with temperatures ranging from -100 °C to +300 °C (-148 °F to 572 °F).

iglide IC-05A is available in dark blue and suitable for applications involving food contact. It meets the relevant requirements of the FDA and EU Regulation No. 10/2011.

iglide IC-05PF offers nearly all the same mechanical properties as IC-05A, but is PTFE-free, PFAS-tested, and comes in a brighter blue color.

This allows material selection to be tailored to the specific requirements of each application. The key is to consider material properties and operating conditions together.

The coating materials are not only available as powders for processing. Select iglide materials are also available as pre-coated sheets and mesh.

Powder coating or ready-coated mesh and sheets?

Coating existing components is not always the preferred option. For applications where ready-made materials are more suitable, igus also offers selected materials as pre-coated sheets and mesh.

The coated wire mesh and steel sheets can, in some cases, be cut to the required shape and formed independently. This makes them easy to integrate into existing systems to reduce wear and friction between components. One example is package chutes, where the materials help packages slide smoothly through the system without getting stuck.

Sheet of powder-coated wire mesh from igus

Depending on the application, different options are available, from coating an existing metallic component to using materials that are already coated.

The right coating starts with the right material selection

Addressing PFAS and PTFE is not just about material composition. What matters is which properties a coating needs to deliver in a specific application and which materials are suitable for meeting those requirements.

With IC-01PF and IC-02PF, igus is expanding its coating portfolio with two PTFE-free variants tested for selected PFAS substances. Together with the other iglide coating materials and pre-coated sheets and mesh, they offer a range of options for industrial applications.