0:48
igus® US Bike Tour Mexico X Brazil Send Off
What an incredible journey it has been across the States! From the sun-drenched boardwalks of California to the historic monuments...
0:48
What an incredible journey it has been across the States! From the sun-drenched boardwalks of California to the historic monuments...
1:02
After the coastal vibes of Narragansett, Providence felt like the perfect urban next stop for the igus:bike tour. Caitlyn jumped...
1:00
For this next exciting portion of the tour, the igus:bike made its way back north, landing right in Rhode Island!...
2:11
The final stage of the U.S. leg of the igus:bike tour brought the bike back to where the heart of...
0:27
Stephen Bowman led the igus:bike through a rainy and foggy tour of Washington, D.C., using the damp conditions to highlight...
1:32
For one unforgettable journey, the igus:bike hit the open roads of the United States, crossing mountains, deserts, and city skylines...
0:53
No trip to Santa Cruz is truly complete without a stop at the famous Santa Cruz Beach, which is exactly...
After the trip through Hollywood and facing the steep inclines of L.A., it was time to hit the beach to...
1:40
Chris and Philip zipped straight to DVO Suspension in Santa Clarita, CA. DVO manufactures high-performance components for mountain bike suspensions...
0:36
Chris and Philip rolled into Las Vegas late Sunday night, ready to turn in and rest up for the gauntlet...
3:02
The trikes manufactured here are life-changing, built specifically for riders with muscle deficiencies, prosthetics, or other disabilities that might restrict...
0:38
The trikes manufactured here are life-changing, built specifically for riders with muscle deficiencies, prosthetics, or other disabilities that might restrict...
1:20
Chris Sandven has been with igus® nearly nine years as a Territory Sales Manager for Colorado, Utah, and Wyoming. He...
2:13
The second stop on the U.S. leg of the igus®:bike tour saw our riders trek across the sunny state of...
0:54
The second stop on the U.S. leg of the igus®:bike tour saw our riders trek across the sunny state of...
Learn how thermoplastics are shaking up the bicycle industry and allowing for lighter and more cost-effective bikes to be designed...