How to choose the right wear ring for your application

When it comes to choosing the right wear ring, the devil is in the details. Slot design, fixing groove depth and width, and material all play an important role in the performance and lifetime of the component. In this blog post, we'll fill you in on what you should consider when selecting the right wear ring for your application.

Mechanical requirements for wear rings: pressure, speed and lubrication

The most important factor in the selection of wear rings is the pressure (force per area), which acts on the rings in the application. But frequency and speed of movement also play a major role. The type of lubrication and the coefficient of friction should be taken into account too. But why are these values so important? Wear rings that are exposed to high pressure should be made of the most resistant material possible. Self-lubricating fiber-reinforced plastics or steels are commonly used here; however, they have the disadvantage of being heavier and requiring constant lubrication. Speed of movement also plays a role. Depending on the material used, if the product of speed and pressure is too great, the resulting frictional heat cannot be sufficiently dissipated without additional lubrication. The type of lubrication depends on application requirements and the technical characteristics of the wear rings in question. Wear rings made of plastic or plastic fabric are often self-lubricating. Solid lubricants such as PTFE or molybdenum sulphide (MoS2) minimize coefficients of friction and protect the rod or cylinder from wear.

Wear ring shape and dimensions

Wear rings can be mounted in two ways. They can either be fitted on shafts or rods or installed as guides in cylinders. This is why guide rings are slotted -- to provide the necessary clamping force and flexibility. Wear rings also serve as a sealing function or are designed to let lubricating or hydraulic oil through (depending on the shape of the slot). There are also angled and straight slots or form-fitting variants with a Z or tooth profile. Wear rings made of plastic offer the advantage of less complex shaping since plastics can be processed and machined relatively easily and cost-effectively.

Material variety for wear rings

The world of plastics has an especially wide range of materials. Not all of them are suitable for wear rings though. Additives are also required to specifically optimize the material properties for use in wear rings. In addition to improved properties such as elasticity, coefficients of friction, and mechanical stability, the materials differ primarily in their temperature resistance, thermal expansion, and chemical resistance. The properties mentioned above, mechanical strength and elasticity, maximum PV values, and thermal properties can be compared especially well by means of data sheets. But what do they say about component durability and service life? Here the comparison is often difficult. Design programs and formulas can help here. For assistance choosing the right high-performance plastic wear ring for your application, contact us here or call us at (800) 521-2747. You can also learn more about our maintenance-free iglide bearing materials here