What is a clevis?

On this page

In the vast world of mechanical components, clevises stand out as versatile and essential elements in various applications. These simple yet effective devices play a crucial role in connecting different components, providing flexibility, and facilitating movement in diverse mechanical systems. This blog will delve into the intricacies of clevises, exploring what they are, how they are used, and the different types available.

Clevis definition: what is a clevis fastener?

a standard U-shaped clevis with a clevis pin and circlip for fasteningA clevis is a type of fastener that most often consists of a U-shaped piece with holes at each end and a clevis pin that passes through the holes. The design of a clevis allows for articulation or movement at the joint, making it an ideal component for applications where flexibility and adaptability are required. The  main components of a clevis are the clevis itself, the clevis pin, and a tang or clevis mount. The clevis pin is inserted through the holes of the clevis, and sometimes held in place with a split pin or a circlip. The clevis pin holds the tang in place between the “prongs” of the clevis.

How clevises are used

Clevises are used in a variety of different applications. Below are some of the most common.

Linkage Systems: Clevises are commonly used in linkage systems where they connect rods, levers, or other components. This linkage allows for the transmission of force or movement between different parts of a machine.

Control Systems: In control systems, such as those found in aircraft or industrial machinery, clevises are employed to create adjustable connections. This enables precise control over the movement of control surfaces or other critical components.

Tie Rod Assemblies: Clevises are integral in tie rod assemblies, providing a secure and adjustable connection between the tie rod and other components. This is crucial in applications where tension or compression forces need to be managed.

Automotive Applications: Clevises find use in various automotive applications, including brake systems and suspension components. They contribute to the smooth and controlled movement of different parts within these systems.

Read more: Plastic bearings & clevis joints for pipe organs

plastic clevis joints being used within a pipe organ

igubal® clevises were the ideal choice for this pipe organ application, damping vibrations and eliminating routine maintenance

Clevis types

Not all clevises are the same. Different types of clevis fasteners are used depending upon application requirements. The most common types are shackles, brackets, clevis hangers and clevis rod ends. 

Shackles: The “standard” clevis, clevis shackles are what most people will first think of when clevises are discussed. They use the classic U-shaped design, along with a tang and clevis pin. 

Brackets: Clevis brackets are similar to shackles in design, with the biggest difference being its rectangular shape rather than being U-shaped. The rectangular hook has holes that can be used for bolts or screws. Brackets are most commonly used within cars or aircraft. 

Clevis hangers: Clevis hangers consist of two clevises: a standard U-shaped clevis and a V-shaped clevis. These two clevises are connected with a clevis pin or other similar fastener. They’re most often used to suspend pipes from a ceiling or other elevated support. 

Clevis rod ends: Clevis rod ends (also called yoke ends) use the same U-shaped hook found in many other types of clevis. The key difference between clevis rod ends and other clevis fasteners is the hole at the base of clevis rod ends. This hole is often threaded in machined parts to provide additional stability.  

An assortment of clevises and clevis rod ends, some with pins already fastened

Plastic clevises versus metal

In many applications, you’ll find metal clevises being used. This is both because of the prevalence of metal options, and assumptions about metal compared to alternatives like plastic. However, tribologically optimized plastic clevises — like those from igus® — offer a number of advantages over metal alternatives, like maintenance-free operation, resistance to corrosion, vibration-damping properties, and weight reduction of about 80%.

Maintenance-free operation: igus’ plastic clevises use tribologically optimized polymers (triboplastics) with embedded solid lubricants all throughout the material. This eliminates the need for any sort of external lubrication, and therefore routine maintenance. The lack of grease or other external lubricants also helps resist dirt & dust.

Corrosion-resistance: The plastics used in igus’ components are resistant to corrosion, making them ideal in applications with frequent exposure to moisture or chemicals. These triboplastics can also resist weak acids and alkalis and do not suffer any structural deterioration when exposed to them.

Weight reduction: It’s no surprise plastic weighs less than metal. This difference is often as much as 80% in the case of igus’ components. This is particularly important in automotive or aircraft applications where weight is one of the most important considerations for engineers.

Vibration-damping: Triboplastic clevises are designed to damp noise and vibrations common in the heavy-duty applications most clevises are used within. This can help extend the total service life of the component, as well as improve overall performance. 

Read more: 6 lesser known benefits of engineered plastic bearings

Conclusion

Clevises, with their simple yet effective design, play a vital role in connecting components and facilitating movement in a wide range of applications. Whether in machinery, automotive systems, or aerospace, the versatility of clevises makes them indispensable. By understanding the types of clevises available and their applications, engineers and designers can make informed decisions to optimize the performance and reliability of their mechanical systems.


Frequently Asked Questions

Clevis FAQ Section

The main function of a clevis is to connect two different components, typically a rod or a cable, to allow for articulation (movement and rotation) at the joint while still transmitting force.

The three main components are the clevis (the U-shaped or rectangular body), the clevis pin (which passes through the holes), and the tang or clevis mount (the part secured between the clevis’s “prongs”).

A clevis pin has a smooth, unthreaded shank and is held in place by a cotter pin or circlip. A clevis bolt has a partially threaded shank that is secured with a nut, offering a tighter, more rigid connection, and is often used for higher load-bearing applications.

Yes, clevis fasteners are widely used in heavy-duty applications, particularly in construction machinery, material handling equipment (like cranes), agricultural implements, and suspension systems, due to their strength and ability to manage tension and compression forces.

A clevis rod end (or yoke end) is a specific type of clevis fastener that features the classic U-shaped yoke but has a threaded or unthreaded hole at the base, allowing it to be directly attached to a rod or actuator.

You would choose a plastic (or triboplastic) clevis for applications where maintenance-free operation, corrosion resistance, vibration damping, or weight reduction is critical. Unlike metal, plastic options often require no external lubrication

Yes, a shackle (often referred to as a clevis shackle) is considered the most common, or “standard,” type of clevis. It features the classic U-shaped design and is secured with a clevis pin.

Clevis hangers are commonly used in industrial and commercial plumbing to suspend pipes from ceilings or elevated structural supports, allowing the piping system to have a secure yet slightly flexible anchor point.