Low-Cost Automation Solutions to Keep Workers Safe and Your Business’s Financials in Check

Photo: "Forktruck Driver" by jaymarable, licensed under CC BY 2.0
If the COVID-19 pandemic has affected operations at your industrial company, you’re not alone. A survey done by the National Association of Manufacturers earlier this year found that more than 53% of respondents anticipated a change in their operations in the coming months, including evaluating work schedules.
To address the issue, PwC, the second-largest assurance, tax and advisory services network in the world, recommends considering automation solutions to reduce the number of workers inside your warehouse.
If you’re new to industrial automation, read these blog posts about the types of industrial robots and benefits of automation for small and medium-sized businesses. Then, read on to learn about specific igus® solutions that can save you money, increase production, and keep your employees safe.
drylin® Gantry Robots
drylin® gantry robots cost up to 40% less than traditional gantries. They’re designed with drylin® linear actuators that feature highly engineered, self-lubricating sliding plastic liners instead of recirculating ball bearings. That innovation helps keep the system lightweight, maintenance-free and corrosion resistant. Additionally, no ball bearings means smoother and quieter operation.
igus® offers drylin® ZLW single-axis linear actuators as well as customized drylin® gantry solutions based on customer-specific application and installation parameters. Plus, you can choose between different stroke lengths and accessories, such as couplings and motor flanges.
Typical applications include pick and place, sorting, labelling, measurement, inspection automation, and repetitive material handling.
drylin® Delta Robots
Our drylin® delta robots (available in 360mm and 660mm sizes) are designed with the same linear actuators and sliding plastic liners as our gantries. They start under $6,000 -- compared to the $20,000+ price point of our competitors -- and do not require any maintenance.
No external lubricants are required and switching out the liners is an easy process. These liners, as well as the other igus® plastic components that are designed into our delta robots, make the system lightweight, quieter than metal, and much more cost-effective.
You can choose between our proprietary robot control software or a more modular software offered by our partner that’s easier to integrate and change over time. Accessories, such as stepper motors, inductive sensors and motor flanges, are also available.
Delta robots are ideal for belt transfer stations, sorting systems, small parts handling, and fast positioning machines.
What’s to Come
Of course these robots may not be the ultimate solution to your operational problems, but they’re something to consider as the number of positive COVID-19 cases continues to rise in the US. Plus, many industries have already embraced automation, making it crucial for you to eventually give your business a competitive and technical advantage over the competition.
To learn more about low-cost automation solutions from igus®, visit our webpage. Or, contact our Low Cost Automation Specialist to order your drylin® gantry, delta or robotic arm today. We also offer maintenance-free automation solutions specifically for material handling -- learn more about them here.