Helical gears vs spur gears & their applications
Gears can come in all sorts of shapes and sizes. Every type of gear has specific applications they’re ideal for, and typically gear designs vary enough that there isn’t much overlap. However, some gear types are rather similar in design and can be used in comparable applications. This blog will look at one such case — helical gears vs spur gears — explaining some of the differences between the two and the types of applications each are best suited for.
Spur Gears
Spur gears are the most common type of gear. If you were to ask someone to describe what a gear looks like, they would almost certainly describe a spur gear. One reason for this would be the simplicity of its design; straight teeth that can interlock with other spur gears, evenly spaced around a circular body.
One of the advantages spur gears hold over helical gears is manufacturing cost. Thanks to the simplicity of design, spur gears are very cheap and quick to manufacture. The point of contact is also smaller with spur gears due to the straight design of the teeth, generating less friction and increasing efficiency. At higher speeds, however, spur gears generate much more noise and vibration than helical gears, making spur gears better suited for low-speed applications.
Spur gears find use most often in applications such as clocks, washing machines and dryers, as well as “gear pumps” which can be used to displace/transport fluids. Gear pumps are most commonly used in hydraulic power applications and applications handling viscous, potentially dangerous chemicals.
Helical Gears
Where helical gears differ from spur gears is the shape of the teeth; helical gears use angled teeth instead of straight teeth. This angle creates a larger, more gradual surface of contact between the gears, ensuring quieter and smoother operation than spur gears. The design also makes helical gears better suited for high-load applications. However, helical gears generate axial thrust due to the angular teeth, requiring either a thrust washer bearing or the combination of two helical gears to create a single gear, similar in design to a herringbone gear.
The key difference in potential applications between helical gears and spur gears is the ability of helical gears to be used in non-parallel shafts. The slanted design of the teeth allows for perpendicular meshing of the gears, opening up a range of potential applications such as in conveyors and elevators, gearboxes for the automotive and printing industries, and more.
If you’re looking for spur or helical gears for your own applications, igus has you covered. We offer bevel and spur gears in a variety of modules and dimensions, as well as custom gears via 3D printing, injection molding or mechanical manufacturing. If you have any questions about iglide gears or materials, you can contact an iglide expert here, or call us at 800-521-2747.