Solar-powered vehicle vs. Australian desert: students prepare for world record attempt

Students from a German university are building a solar vehicle to be powered by the blazing sun in an Australian desert in hopes of setting a Guinness World Record.
Students at Bochum University of Applied Sciences are building the solar buggy, which they call a “Froggee”, for the 224-mile jaunt across the Simpson Desert. The team is hoping to beat the existing standard of 4 days, 21 hours and 23 minutes, which was set in 2017. The race from Purni Bore to Birdsville will be held in 2019.
“We wanted to take solar mobility off-road and use solar energy in an area it is suited best: the desert,’’ Birgit Reuter, a member of the 16-student team, said.
Bochum students have been building solar vehicles since 1999.
“It was just a small step for us to go from an Australian road to the Australian desert. And, there are not exactly a lot of deserts in Germany,” Reuter said.
The vehicle the students are designing is a compact, two-seat buggy that will be powered entirely by the sun. It includes a 40m² solar array that consists of 144 panels and 1,052 silicon cells. Students are using 96 lithium ion pouch cells for the battery. Like most of the products in the vehicle, the battery is extremely light.

“We don’t have any infrastructure in the desert, so we’re charging within three hours via a 40m² foldable solar array,’’ Reuter said. “This is basically our charging station to go. The energy is stored in a battery, just like any electric vehicle.”
Reuter said the vehicle’s output voltage is 650V at 6kW and 9.2A.
“With it, we can be fully charged within three hours,’’ she said. “We believe the buggy will be able to drive 100-150 kilometers on one charge, but frankly, we will just have to test it to see how far it can go.”
Devising the power source for the vehicle has proven to be just one of the challenges for the students. Another significant hurdle is finding lightweight components that can stand up to the heat, terrain and desert conditions.
“The desert is quite demanding, and we frequently couldn’t just take any parts that might fit the specs of the vehicle,’’ Reuter said.
The different desert surfaces, such as mud, rocks, erg, and dunes, will test the durability of the vehicle’s components. Stopping the infiltration of sand poses one of the most perplexing design challenges.
“There will be a lot of sand around that acts like sandpaper and gets into the smallest holes,’’ Reuter said. “The electric box will need to be tightly closed and all outer parts need to be at least IP65.”
IP65 is a standard established by the Electro-Technical Commission for Ingress Protection. IP65 means the assembly is totally protected against dust ingress.
The buggy includes two motors for each axis and a controller for each motor. The unit includes 10 chainflex® cables manufactured by igus®, a German-based company that runs its North American operations out of a facility in East Providence, RI. Those 10 cables connect the battery to the controllers and the controllers to the motors.
The cables are also shielded, oil-resistant, flame-retardant and are suitable for temperatures up to 176 degrees Fahrenheit. The cables span 15 meters in the vehicle. The shield in the cables was one of the key advantages in selecting the component.
“We needed a shielding in our motor cables because the motor controllers are inverters and bring out alternate current to the motors,’’ Reuter said. “In this field, it is essential to have good shielding to prevent electromagnetic compatibility (EMC) problems. We needed cables that are very robust and durable and at the same time conduct 400 volts. Since space is tight, they also needed to be bendable.”
Reuter said in building the buggy prototype, students faced issues in getting the electrical components to work together along with the controllers. They also needed to acquire special components to build the axles.
Even with all of their planning and attention to detail, there is no way of determining how the “Froggee” will survive the sizzling desert heat. Temperatures can reach as high as 122 degrees.
Simpson Desert covers 68,000 square miles and is home to the world’s largest sand dune desert. Some of the best four-wheel driving in Australia takes place in the Simpson Desert, an area popular among tourists. No maintained roads cross the desert, which averages less than six inches of rain per year.
Students from Bochum’s mechanical and electrical engineering are spearheading the vehicle’s construction team with support from students in computer science, business, economics, and sustainability. The vehicle for the 2019 race is still under construction, but Reuter said the team is ready to challenge the existing record.
“Our vehicle is specifically made for these conditions, so we believe we will definitely be faster,’’ Reuter said.
More information about the team is available on its website and Facebook.
Update: After traveling about 43 miles in the Simpson Desert, the students had to break off their world record attempt due to extreme heat that made it “practically impossible” to charge the buggy’s battery, according to the team’s website. The team states that the buggy had no technical problems and could easily drive through the sand. They list some main takeaways from their experience on their website:
- The buggy is absolutely suitable for the desert
- A solar self-sufficient crossing of the desert is realistic
- A well-functioning team can achieve an incredible amount
- There are always unpredictable variables
- There are incredibly great people all over the world
- Even dangerous snakes and spiders find the area uncomfortable and rarely run into them
- Wandering, wild donkeys are very loud
- The distant howl of dingoes is daunting
- Appreciation for showers and toilets has increased