How to Make a Linear Actuator Move Faster

September 17, 2021 Shizu Yamaguchi

Here, we’ll cover two ways to increase the speed of your linear actuator. But first, note that the linear actuators referred to in this article are known as slide tables and linear slides. Advice for their rod-end counterparts is not covered in this article. With that caveat out of the way, let’s get started.

For screw-driven linear actuators (pictured right), change the lead screw’s pitch to increase speed. For example, instead of using a standard 10×2 pitch, increase it to 10×5, 10×10 or even 10×50. That way, for every rotation of the lead screw, the carriage can travel that much farther. A single rotation of the 10×5 lead screw would increase carriage distance by 3mm, the 10×10 would increase distance by 8mm, and so on.  

Screw-driven systems generally have a variety of speeds at which they can go. One way to find out maximum speeds for your application is to use an online configurator. For igus® linear slides, maximum speeds range between 0.018 m/s and 0.333 m/s.

There are limits to the speed of a screw-driven system, however, since screws start having issues when they reach the upper limits of their speeds. Lead screws might start to whip, for example.

The second way to increase the speed of a slide table is to swap out a lead screw system for a belt drive system. Belt-drive systems offered by igus can go up to about 5 m/s.

Belt-driven linear actuator

To learn more about whether a slide table from igus could meet your needs, please reach out to us by phone at (800) 521-2747 or visit our website.

Previous Article
Lead Screws and Polymer Nuts for the Packaging Industry: Convert Rotary Motion into Maintenance-free Linear Motion
Lead Screws and Polymer Nuts for the Packaging Industry: Convert Rotary Motion into Maintenance-free Linear Motion

Leads screws with metal nuts may have been your go-to solution in the past, but opting for high-performance...

Next Article
How can I recognize the thread direction of my lead screw?
How can I recognize the thread direction of my lead screw?

The thread cutting direction right or left can be easily determined with a visual inspection. In this blog ...