Key parts of an electric motor

Electric motors are the leading source of electric energy usage worldwide, accounting for roughly 45% of global electric energy consumption. They power everything from household appliances like blenders and fans to industrial machinery and electric vehicles. While they may seem complex, their operation is based on a few key components working together to convert electrical energy into mechanical motion. The core parts that make this happen are the stator, the rotor, and in many cases, a commutator.

Cutaway view of the internal structure of a motor, with the commutator, windings, rotor, and stator all labeled

This blog will break down what each of these components does and how they interact to make an electric motor function.

Related: Choosing the right motor for your application

What is a stator?

The stator is the stationary part of an electric motor. It can be thought of as the outer casing or frame that houses the primary electrical components. It’s typically made from laminated steel to help concentrate the magnetic field and is lined with coils of insulated wire called windings. The windings are where electrical energy is supplied to the motor.

An electric motor stator on a plain white background

When an alternating current (AC) is sent through the windings, a powerful magnetic field is created. The design of the stator’s windings and the way the current flows through them causes the magnetic field to rotate — forming the core principle of motor operation. 

The spinning magnetic field of the stator interacts with the rotor, which is the rotating part of the motor housed inside the stator — except in the case of outrunner motors, where the rotor is located outside of the stator. The interaction of these two components is what generates the torque that makes the motor spin.

What is a rotor?

The rotor is the rotating component inside an electric motor. The rotor is typically made from a laminated steel core to enhance its magnetic properties and is mounted on a shaft that extends outside the motor’s housing. This shaft is what connects to a load to deliver the motor’s power.

An electric motor rotor on a plain white background

A rotor’s function is based on the fundamental principle in magnetism that opposite poles (positive/negative) will attract, and like poles (positive/positive or negative/negative) will repel. The rotor’s own magnetic field interacts with the rotating magnetic field of the stator to facilitate the motor’s motion.

As the stator’s magnetic field rotates, it exerts a force on the rotor, causing it to try and “catch up” to the spinning magnetic field. This constant pushing and pulling force on the rotor is what creates the continuous rotational motion that drives the machine the rotor is connected to. 

What is a commutator?

A commutator is an essential component in most direct current (DC) motors. It’s an electrical switch made of copper segments arranged in a ring. Two brushes — stationary electrical contacts often made of carbon — press against the commutator to supply power to the motor’s coils. 

The commutator is used to periodically alternate the direction of the electric current flowing into the rotor. If the current always flowed in the same direction, the rotor would make a single half-turn and then stop. A commutator changes the direction of the current at the precise moment needed to keep the rotor moving in a single, continuous direction.

An electric motor commutator on a plain white background

Brushless DC (BLDC) motors do not use commutators, instead relying on an electronic controller that uses semiconductor switches (transistors) to reverse the direction of electric current as needed. Brushes require sliding contact to function, so BLDC motors generate less friction and improve service life compared to brushed DC motors by eliminating them. This reduced friction translates to about a 10% difference in overall efficiency.

White Paper: 11 tips for selecting the right motor control unit

A white paper thumbnail depicting four different motor controllers from igus on a white and orange background

Conclusion

Understanding the function of the stator, rotor, and commutator is key to comprehending how electric motors convert electricity into motion. The stator's stationary magnetic field interacts with the rotor's own magnetic field to generate the torque that makes the motor spin. This fundamental interaction of magnetic fields is what drives the continuous rotational motion of a motor. For brushless motors, commutators are necessary to change the direction of current and keep the rotor moving in a single, consistent direction.


Frequently Asked Questions

motors FAQ Section

The primary components of an electric motor that work together to convert electrical energy into mechanical motion are the stator, the rotor, and often, a commutator.

The stator is the stationary part of an electric motor, typically made of laminated steel and lined with insulated wire windings. When alternating current (AC) is supplied to these windings, it creates a powerful, rotating magnetic field that is essential for the motor's operation.

The rotor is the rotating part of the motor. It's mounted on a shaft that connects to a load to deliver power. The rotor's magnetic field interacts with the stator's rotating magnetic field, causing a continuous pushing and pulling force that makes the rotor spin. This is based on the principle that opposite magnetic poles attract and like poles repel.

A commutator is an electrical switch found in most direct current (DC) motors. Its main purpose is to periodically change the direction of the electric current flowing into the rotor. This is crucial because without it, the rotor would only make a single half-turn and then stop. The commutator ensures the rotor continues to move in one consistent direction.

Brushed DC motors use a commutator and brushes to supply power to the motor's coils and reverse the current's direction. Brushless DC (BLDC) motors, on the other hand, do not use a commutator or brushes. Instead, they rely on an electronic controller with semiconductor switches to reverse the current as needed. Eliminating the brushes reduces friction, which can improve the motor's service life and increase its efficiency by about 10%.

Magnetic fields are fundamental to the operation of an electric motor. The stator creates a rotating magnetic field which interacts with the magnetic field of the rotor. This interaction of magnetic fields generates the torque that causes the motor to spin continuously. The rotor constantly "chases" the spinning magnetic field of the stator, which produces the continuous rotational motion that drives the connected machinery.

The rotating magnetic field of the stator is the core principle of motor operation. This field interacts with the rotor's magnetic field, exerting a force that causes the rotor to try and "catch up" to the spinning field. This constant force is what creates the continuous rotational motion necessary to drive the machine or device the motor is connected to.

Electric motors are a leading source of electric energy usage, accounting for about 45% of global consumption. They power a vast range of devices, from common household appliances like blenders and fans to industrial machinery and electric vehicles.