about 7 years 7 Guidelines for Cable Installation Review 7 rules to maximize service life and performance of cables in your next application. Read Document
1:06 about 7 years Robot cable igus'' blended sheath cable with a flexible core for robotic applications. Watch Video
0:09 about 7 years How to install cables into split crossbar cable carriers Cables can simply be pushed into the cable carrier via a flexible opening in the crossbar ("E-Z Chain"). Watch Video
2:23 about 7 years igus® test lab Take a look inside the igus test lab and see how the company tests its cable carriers and continuous-flex cables. Watch Video
1:58 about 7 years chainflex® continuous-flex cables vs. other types A comparison between chainflex® continuous-flex cables from igus versus so-called ''chain-suitable'' cables. Watch Video
0:47 about 7 years Introduction to the igus® Pneumatic Retraction System at IMTS Jeremy Biltz from igus inc introduces and explains the features of the Pneumatic Retraction System. This system allows the cables to wrap neatly around the different axes. Watch Video
1:36 about 7 years Guaranteed against failure – the igus® testlab for cable movement Detailed fly-through of the igus® chainflex® 29,600 square foot test facility in Cologne, Germany. Over 2 billion test cycles per year and 650 test can be performed simultaneously. Up to 36 months gua Watch Video
0:53 about 7 years HMI2016 readycable® 4000 drive cables available readycable® and readychain® Product Manager Marcel Lamers explains the wide selection of igus® harnessed cables as well as the available online product finder. Click here to learn more about ReadyCab Watch Video
0:54 about 7 years New Cable Jacket Stripper Check out the newest addition to the igus® Inc. warehouse in action! Watch Video
1:44 about 7 years 7 basic rules for cables in motion Motion plastics specialist, igus, has more than 25 years’ experience developing and producing cables for moving applications. Over 2 billion double strokes are carried out in its 29,600 sqft test lab Watch Video
1:20 about 7 years Project highlight: Cables and Cable Carriers on the Memorial Bridge, Portsmouth, NH In 2014 the memorial bridge originally designed in 1922 by J.A.L. Waddell was replaced by a new bridge with cutting-edge technology. The new design maintains the spirit of the old design, but employs Watch Video
0:47 about 7 years igus® cable cutting part 2 igus® harnessed cable assemblies are cut precisely using best-in-class Schleuniger cable processing equipment to ensure consistent length with high tolerance precision. Check out the loading operati Watch Video
0:50 about 7 years Quality features of a high-end bus cable Learn more on our website! www.igus.com/chainflex Watch Video
0:33 about 7 years igus® cable cutting part 1 igus® harnessed cable assemblies are cut precisely using best-in-class Schleuniger cable processing equipment to ensure consistent length with high tolerance precision. Featured here is the Schleuniger PowerCut 3700 cutting machine for precise cutting of cables with diameters up to 25 mm. Cable is fed to the cutting machine by a Schlueniger PreFeeder 4300 prefeeding machine that can take on cable reels of up to 880 lbs (400kg)! Watch Video